This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电量计芯片的电压校准问题

Other Parts Discussed in Thread: BQSTUDIO

使用电量计芯片bq27520之前,通过bqStudio校准电压,详细是用万用表测量电池两端电压后在Calibration窗口下进行校准,请问这个校准电压的动作是要在放电状态下还是无负载的状态下进行?

 

在无负载状态下校准电压后,发现在充放电状态下,软件的电压值和实际电池的电压值差别较大;

例如在1A恒流放电状态下,软件显示电压为3663mV,而实际电压表测量电池电压为3613mV;

在2A恒流充电状态下,软件显示电压为3985mV,而实际电压表测量电池电压为3870mV;

 

请问如何解决电池电压误差大的问题?附上原理图: