This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于电平转换芯片的推荐

Other Parts Discussed in Thread: TXB0108, TXS0108E
【求助】关于电平转换芯片的推荐

我需要一款电平转换器件连接16位并行adc和mcu,条件如下:
1.ADC使用LTC2270,输出为1.8V的cmos,高电平为1.79V(输出电流-500uA下测得),低电平为0.01V(输出电流500uA下测得),MCU为3.3V供电,输入高电平需大于2.31V,输入低电平需小于0.99V,输入电流最大+-5mA左右
2.一共有32路信号,可以用4片8路总之可以多用几片,每通道的速率可以达到8MHZ。
3.电平转换芯片的输入电流怎么确定?看到好多数据手册上都没有写。
请推荐一款适合的电平转换芯片,本人现在想使用TXB0108。