This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2951输出电阻配置问题



在贵司申请了LP2951ACMM/NOPB样片 。

根据数据文档说明Feedback上电压是1.235V,需要设置Feedback接地电阻和上拉电阻分别是120K和56K ohm,才能输出1.8V电压,。

但是我测量芯片上Feedback到Gnd的电阻发现引脚内部阻值是50K,所以只要把Feedback上拉25K到output恰好输出1.8V电压。

我在数据文档里并没有发现Feedback有50K的下拉电阻相关的描述,请问这个是文档的错误还是芯片的问题?