This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27510-g3 SREC is corrupt



HI ti:

We encountered some problems when using bq27510drzr-g3. The specific phenomena are as follows:

1. After the  file is burned, it is found that several cycle meters are normal at the beginning. After a period of time, part of the equipment appears bq27510-g3 unable to accurately read the phase

The data, or the SREC file, is corrupt. The probability of occurrence is about 5%. Restarting the device does not return to normal.

2. If you burn the OK SERC file again, everything is working normally, which means that bq27510-g3 is not damaged. So it turns out that the SERC file is corrupted. I want to know

Under what conditions, the SERC file is corrupted.

3. How to check this problem? Because the probability is low and it is not easy to reproduce. According to your experience, is there any way to analyze and eliminate it?

4. Can SREC documents be analyzed to identify problems? Is there any problem in the production of SERC files? The attachment is the SERC file.

5. We use stm32l476vgt6's pin ﹣ 95 to connect gas ﹣ SCL and pin ﹣ 96 to connect gas ﹣ SDA. The following is the circuit diagram.