This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

采用BQ27520YZFT-G4电量计,电量显示不准,请问如何做电池建模。



您好,

我们项目是高通450平台,充电IC采用BQ25890HRTWT,电量计采用BQ27520YZFT-G4。

现在充电IC已经调通了,也可以充电,但是电量显示不准确,电量停在98%之后就再不涨了。

我们的电池规格如下:单锂聚合物电池,容量:2750mAh,标称电压:3.8V,满电电压:4.35V,充电电流:0.5C,最大放电电流:0.5C。

请问下如果要对电量显示比较准确的话,是否要对电池进行建模,测量电池的曲线。

你们有没有类似规格电池的参数?

如何才能得到准确的电量值?

谢谢!