This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561 FullChgCap在电池学习的时候log显示有7738mAh 但是srec文件烧录到电量计里面系统读到只有5277mAh



1.如题,循环学习成功后,log显示FullChgCap有7738mAh,实际是8000mAh,相差不多。但是系统起来后只能读到5277mAh,不应该是7738mAh 吗?量产srec文件有记录学习到的容量信息吗?

[14768.991736] healthd: battery l=27 v=3487 t=35.8 h=2 st=3 c=-1066 fc=5277000 cc=0 chg=

2,terminate voltage参数设置的是3.0V,实际关机电压是3.4~3.5V。是不是应该把terminate voltage设置成3.5V?