This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59282 贴近市场需求

Other Parts Discussed in Thread: TLC59282

       TLC59282产品本着更贴近市场的需求满足受众的需要,并且多项标准目前在同类产品达到无可替代的地位:通道间的电流误差精度:±0.6%(典型值);器件间的电 流误差精度:±1%(典型值);最小30nS BLANK脉冲宽度可在多路复用应用中实现更高的刷新频率三项指标达到业界唯一水平。

TLC59282 具有分组式通道延迟的16通道恒流LED驱动器

特点

·16通道恒流开关型驱动器

·支持2~4.5mA恒流范围(使用外部电阻器设定) VCC<3.6V时为2~3.5mA

·3.0V至5.5V输入电压范围

·通道耐压高达17V

·通道间的电流误差精度:±0.6%(典型值)

·器件间的电流误差精度:±1%(典型值)

·支持最小30nS BLANK 脉宽 来控制OUTn的开关

·35MHz数据传输速度

·DBQ(SSOP)封装,24引脚

优势

·分组式通道延迟(4通道一组)可最大限度地降低同步开关噪声,并可实现简洁的PCB布线;

·通道间、芯片间电流匹配高,使得各串LED之间的亮度有效保持一致;

·最小30nS BLANK脉冲宽度可在多路复用应用中实现更高的刷新频率。

·与Microblock LED驱动器引脚兼容。

应用

·LED视频显示器

·LED留言版

·景观照明与LED指示器