This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM34936电源问题



设计输出100W 标称电压12V;输入8V-16V,设计图见附件;

问题:

Vin=8V时  VOUT=10.19V   5.6A   57W(带载)
                  VOUT=12.09V                    (空载)
VIN=14V时,VOUT=12V  (空载)
                     VOUT=11.06  7A      77W   (带载)LM34936RHFR-SCH.pdf