This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23758 變壓器設計

TPS23758EVM-080 Evaluation Module 這個應用是Input voltage:37~57V
我的需求
input voltage:16V ~57V

DC-TO-DC CONVERTER
output voltage:5V

output current:2A

請問變壓器怎麼修改,或是可以提供目前使用T2 LDT1018-50R的變壓器結構圖
我自行修改