This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

learing clycle QMAX UPDATE

Other Parts Discussed in Thread: BQ40Z50

您好, 

          我用BQ40Z50进行4芯4.2V松下电池串联学习,根据以下学习步骤学习,QMax只能更新到05,反复学习未到06

1. 烧写对应chemid-2072 ncr18650BD(3180mah) 

2.校验参数

3.data memory 相关参数设置design cappacity mAh=3180mAh;design cappacity cWh=4579mWh;design Voltage=14400mV ;DA cofiguration(仅CC0=1;CC1=1;NR=1);FET option(仅CHGFET=1;PCHG_COMM=1);Charge Term taper current=70ma;dsg current threshold=100ma;chg current threshold=50ma;Quit Current=12ma;Term Voltage=12000mV;保留基本保护

4.进行学习:

          4-1.发送0X21允许阻抗跟随 以及发送0X41进行电阻参数更新,此时update status由00变为04

          4-2.放空电量知道终止电压,并开路空置5小时,VOK=0, RDIS=0 ,REST=1 ,Qmax=0

          4-3.用2162mA电流进行充电充满,开始时VOK=1,RDIS=0充满后FC=1,开路空置2小时,VOK=0,RDIS=0 ,REST=1,QMAX=1,此时update status由04变为05

          4-5.用500mA负载进行放电,复制到终止电压为止,然后开路空置5小时,VOK=0,REST=1,QMAX=1,Update status仍然=05,没有更新到06.

这里有几个问题4-3充满时,不需要再次0x41了吧,RDIS应该一直保持为0的状态,可是该步骤里再次提到了RDIS要被清空?其次QMAX更新一次后,一直为1的状态是否正常?最后为什么反复学习仍然不能更新到06呢