Other Parts Discussed in Thread: TPS54360
1、问题1:根据文档slva369a(www.ti.com.cn/.../slva369a.pdf
2、问题2:如下图,设计参考例子里有两个地(一个是三角号,一个是三条横线),是不是图中所有的三角号的地是同一个网络,而三条横线的是另一个网络呢???如果是这样的话,这两个地将来如何连接呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
这款芯片做不到2路都1A输出,建议你用TPS54360,这个芯片的3A版本,计算方法就是按照你看到的这款文档来做。
三角代表的是负压,三横代表的是GND 0V.
TI诚邀你参加全新设计的参评页面测试,参加测试即可享有TI购物9折优惠,点击“ 加入 Analog 产品页面测试 ”报名,名额有限。感谢您的参与。
“加入 Analog 产品页面测试” 链接可见电源板块置顶帖。