This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM26480输出电压的范围和并联使用的问题

Other Parts Discussed in Thread: LM26480

Lm26480's spec said one buck channel output range is 0.8volts to 2volts, another channel buck channel output range is from 1V to 3.3Volts, 

I want two buck channel output voltage is 1 volts, and in parallel. Is there risk?

LM26480的规格书说:一路BUCK的输出电压范围为 0.8V 到 2 V,另一路buck的输出电压范围为1V 到 3.3V,我想两路输出都为1V,输出端并联使用,这样的话,输出电流是单路输出的2倍,这样做有什么风险吗?

  • Hi
    两个DC/DC是电压模式,不可以并联使用,因为无法均流。
    TI诚邀你参加全新设计的参评页面测试,参加测试即可享有TI购物9折优惠,点击“ 加入 Analog 产品页面测试 ”报名,名额有限。感谢您的参与。

    “加入 Analog 产品页面测试” 链接可见电源板块置顶帖。
  • 没有均流电路的恒压源,不建议直接并联使用。不能做大均流或不能一起输出工作。