This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133 在没有上电池的状况下SW依然有输出电压8.4V



实验环境

输入电压12V

2S2P电池 : 8.4V

1. 在系统开机下移除电池,系统判断电池不存在, STAT LED会闪烁, 但SW 8.4V依旧存在, 请问8.4V依旧有输出电压这是正常的吗?

2. 根据问题1,如果8.4V存在,是否可以让它不输出?

3. 后续我把机子在没有接上电池的状况下.重新插拔DC , 量测到SW端的电压是1.1V ,请问这是什么原因?