This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

比如蓝牙芯片CC2640的供电范围是1.8V到3.8V,我想用一套电路给他供电,电路经过调节能输出1.8V到4.2V 那我应该输出多少给蓝牙芯片供电,如果分别用1.8或3.3v供电那这个芯片都能工作,但功耗是不不一样了,一般用多大



谢谢

  • 首先没太明白你的问题,但是我谈谈自己的理解。
    首先两者供电的功耗只要是你不太考虑极低功耗,两个都可以使用。但是需要注意你的蓝牙芯片需要与CPU连接,那么你要注意与CPU连接的IO是1.8V还是3.3V,这个需要与CPU那边IO电平匹配,不然就需要电平转换芯片了。

    如果你自己也不确定,那建议设定为兼容设计,根据实际选择供电电压即可。只是对于一种供电来讲比较麻烦了一点。
  • Hi
    一般常见电压是3.3V,也建议问一下射频的工程师。
    再看你的电压源是多少?才好选择电源转换芯片。