Other Parts Discussed in Thread: LM5022, LM3488
HI
询问下5022最低的开关频率能到多少?能到80KHz吗?还有驱动输出是多少伏的电压,我没查到资料,希望帮忙告诉下!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Datasheet 只是强调了LM5022最高频率可以高达2MHz, 并未提及最低频率,经验上一般最低可以达到几十kHz(50kHz以上), 不过从datasheet 第七页第一个图看datasheet推荐频率是200kHz~1000kHz(接近).
通常而言,对于DC/DC, 频率推荐是300~700kHz, 500kHz 典型值。
频率过高,会导致功耗交大,影响效率,而且导致发热严重。频率过低,会导致电感感量过大,造成零件体积大,而且动态反应慢。
驱动电压输出见datasheet第五页参数表:
Output High Saturation Voltage (VCC – VOUT) 0.25~0.75 V, 即高电平输出是Vcc-250mV(典型值)
Output Low Saturation Voltage (VOUT) 0.25~0.75 V, 即低电平输出是250mV(典型值)
驱动输出电压只有250mV吗?那如何驱动MOS管呢?我看LM3488的驱动电压能到7.5V的啊?LM5022是如何驱动Boost的开关管呢?
如果我LM2055的输入电压是从9V~18V的话,意思是我的驱动输出电压也是从9v~18V吗?像LM3488是描述的再小于7.5V的时候,驱动电压是等于输入电压的,当大于6V的时候是稳定在7.5V的啊,那么LM2055的驱动电压在9~18V之间是什么样子的呢?
Hi
如之前所谈,驱动输出的电压是Vcc-250mV(典型值), 而Vcc的电压见datasheet: http://www.ti.com.cn/general/cn/docs/lit/getliterature.tsp?genericPartNumber=lm5022&fileType=pdf 第六页第四个图.
如果你的电压是9~18输入, VCC电压将一直是7-025mV=6.75V(左右)