如题,想用UCC28951设计一个全桥电源,输入10~16V,200A;输出48~60V,50A,隔离方式!
但TI系统给的仿真工具限制了电压,不好整变压器变比,不咋会计算变压器设计参数
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
变压器计算:输入10~16V~200A,输出48~60V~50A,频率250K
匝比计算:Np/Ns≈1/9.16
典型占空比计算:Dtyp=≈0.577
输出电感电流纹波峰值:▲ILout==10A
原边磁感应计算:Lmag≥443.7nH
这是根据规格书计算出来的参数~~
零点电压电感Ls≥3.25pH
输出电感5.076uH
仿真给出的原边VDS=65V,775A,副边VDS=247V,78A
按规格书中计算原边差不多,副边计算VDS=293.2V
今天又找了另外一份TI得设计36~60转12V,结果发现参考设计和规格书里面有些公式不一样!坑了~~
找了几本国外的书,初步计算,视在功率8081W,ETD59磁芯,材质PC40,Bmax为0.061mt,原边25根2.66mm直径铜线1匝,副边3根2.66mm直径铜线8匝,三明治绕法
Hi
这个设计很麻烦,TI的webench一般都是针对常规个参数设计例如以这个芯片而言一般都是市电或者400V输入。
我觉得用几个升压芯片并联设计或者更简单一些。