Other Parts Discussed in Thread: LM5155
Hi:
当前有个DC-DC的方案需求,DC8~36V输入,输出隔离3组:15V1A(主路), 20V 0.2A,5V 0.3A。全载效率75%以上(在10分钟内每次全载时间小于1分钟,其余时间轻载小于20%),输出短路保护。初步选用了LM5155DSSR,变压器选用PQ2016(AE62 MM2),副档是初步原理图
请师兄帮忙审核可行性?原理结构和变压器?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM5155
Hi:
当前有个DC-DC的方案需求,DC8~36V输入,输出隔离3组:15V1A(主路), 20V 0.2A,5V 0.3A。全载效率75%以上(在10分钟内每次全载时间小于1分钟,其余时间轻载小于20%),输出短路保护。初步选用了LM5155DSSR,变压器选用PQ2016(AE62 MM2),副档是初步原理图
请师兄帮忙审核可行性?原理结构和变压器?
你好 我也想用LM5155做一个升压降压电路,参考技术手册的电路图,输入电压范围18-28V 输出为24V 电流1A 可以实现么?参考以下哪一个比较好?