This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28610 ZCD question

Other Parts Discussed in Thread: UCC28610

Hi Guys

反激使用UCC28610,输出电压12V。测试,170V到400VDC输入情况下,满载的时候ZCD数量都是2。

 问题:

1.为什么170V到400VDC输入,满载(继续增加负载,芯片就处于重启状态了),ZCD数量都是2,为什么没有出现ZCD=1的情况?下面的波形(Picture 1)为400VDC输入电压Load=4A,Mosfet的VDS。测量波形中,反激自由震荡的时间(红色圆圈内)为2.4 us和datasheet中的Twait(ZCD)时间有关系吗?

Datasheet,Page 7

Picture 1  Vin=400VDS, Load=4A, Signal 2 VDS

 

2. 观察上面VDS的波形(Picture 1,Load=4A),MOSFET并没有在谐振的谷底开通Mosfet。负载比较小(Load=3A),ZCD等于5的时候(Picture 2), MOSFET开通时比较接近谷底。

 

负载比较大的情况下(Picture 1,Load=4A),MOSFET并没有在谷底开通Mosfet,是UCC28610的原因造成的吗?我测试了170VDC,250VDC下满载的波形, MOSFET同样没有在谐振到谷底开通Mosfet。

 请问这里是要加入Datasheet中说明的电容来将LC谐振相位调整至于ZCD电流相位相同吗?这里的具体的开通时间点与什么有关系?

Picture 2  Vin=400VDS,Load=3A, Signal 2 VDS

 

3.datasheet中Page27。圆圈内tWAIT的含义是什么?

 这里说明的是不是说IDRV的输出,或者Ton的时刻与第一个检测到的ZCD至少要有7.5us的时间差?

 Thanks

-Vincent