This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930采样线束有阻抗对采样精度有影响吗?

Other Parts Discussed in Thread: BQ76930

     1. BQ76930采用两颗芯片级联,实现20串电池包电压采样,线束有1K欧姆的阻抗,芯片采出来的电压很稳定,不会乱跳动,。但是改成16串,VC3与VC4短接,VC8与VC9短接,如果在与VC3t和VC4或VC8和VC9上下相邻采样线束有50欧姆以上的阻抗,上下相邻的采样电压就会有跳动,最大有200mV。

     2 . VC3t和VC4或VC8和VC9上下相邻采样线束与其串的阻抗一样,保持在50豪欧姆,把板子上IC 前端的1K电阻改成10K,该串的采样电压也很稳压,不会乱跳动。如果把1K电阻改0欧姆,把1K电阻串在线束上,该串的采样电压就会有跳动,最大有200mV,从原理来说,只是把电阻从板上移到线束上,原理上是一样,为什么采的电压会 乱跳动呢?