This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610充电电流不到设计值

Other Parts Discussed in Thread: BQ24610

你好!

我使用的BQ24610给4cell电池充电,充电功能等都正常。

就是设定的充电电流是4A,可是充电电流达不到这个值。

电池14.7V时充电电流2.3A

电池15.3V时充电电流1.5A左右

测量方法是串万用表在电池端。

我理解的是到达16.8V电流才会逐渐减小。这种情况,增大充电电流只能调整预设值了吗?