This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM317A设计问题



1、看资料LM317A可以支持24V转12V,但是用WEBENCH® Designer  在线设计的时候,输出0.5A的电流,设计不能输出。
2、实际设计中,不加负载的时候,输出电压会向上漂移,添加4个1K电阻的负载,电压下降不能与设计值有差异。

  • Hi

         不建议你用LDO来做这个转换,因为功耗太大,6W的功耗,你可以算一下芯片温度,都可以用来烧开水了,效率只有50%,即便你散热做得再好,都没有必要。

         测试电压偏离,可能和layout有关,你需要注意按照datasheet说明来layout,以及注意输入输出电容选取。

         建议用DC/DC来做,很多芯片效率都能达到90%以上甚至95%,只是外围增加一个电感,layout空间稍微大一点。