1.UCC28780 不加Gate driver是否可以?
2.UCC28780 原本有Gate driver是用兩顆N MOS,如果拿掉Gate driver請問也是可以用N MOS嗎?還是要用P MOS接地呢?
3Q~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi~ 感謝你的回覆,
我看TI是推薦UCC27712,請問有類似功能但IC 封裝小於SO8的嗎?目前我耐壓不用到620V,只要100V以上就可以
請問除了線上留言是否有其它方式可以向原廠請教問題呢?比如說可以用mail嗎?
UCC27712好像輸出電壓會大於5V?所以再透過ISO7710FD來降壓?這樣才符合GaN MOS的低驅動電壓?
謝謝~~