This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50 short in discharge



Dear :

        there are two questions:

         the first is about the  "ASCD" setting :

1,       14.9.12.1  Latch Limit  :

          the default setting  data is" 0"   ,in my opintion ,in short circuit of discharge the output is 0 V.

          so the setting is 0 V. is right?

2,       14.9.12.2 Counter Dec Delay :

           the default setting is"10" s; in the short conditation  ,  10 seconds  may be too long ?

3,       14.9.12.3 Recovery:

           14.9.12.4 Reset  :

            could you tell me the difference of the "Recovery " between the "Reset"?

the second :

           how to set if  resease the short condition ,and the output can recovr to normal.

          or if need to charge can be to normal?

thanks 

       

  • 您好,关于ASCD Latch Limit :Short Circuit in Discharge Latch counter trip threshold 是个计数器默认是0
    Counter Dec Delay : Short Circuit in Discharge counter decrement delay 是计数器减量的延迟
    Recovery: Short Circuit in Discharge recovery time短路放电恢复时间
    Reset : Short Circuit in Discharge latch reset time短路放电闩锁重置时间
    如何恢复ASCD保护,请参考TRM 2.7.3ShortCircuitin DischargeProtection
    www.ti.com.cn/.../sluua43a.pdf