Other Parts Discussed in Thread: TPS62170, TPS62150
+5V转-5V,电流200mA,纹波要低一些,50mV以下,请问有合适电源芯片推荐吗?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
选择输入电压10V,负载能力大于400mA的降压芯片都是可以的,例如TPS62170之类,很多芯片都可以。
设计可以参考TPS62150负压输出(TPS62150的不同电流输出版本),在其网站上可以找到。