This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教有关TPS2549几个问题

Other Parts Discussed in Thread: TPS2549

TI 工程师:

你们好!

我想请教几个有关TPS2549这个芯片的问题:

1> 我们在SOC芯片侧只有1路OTG的USB模块,我们想要由1路转换为2路USB,我们使用了一个USB Switch芯片,后接2路TPS2549,当USB Switch导通USB1通路的话,通路1的TPS2549设置为(CTL1-3:111),进入CDP-SDP auto switch mode,此时将R(ILIM_HI) 设置为 19.1 kΩ,即2.8A最大电流,那么这一路给支持快充的安卓手机,苹果手机,以及iPAD分别充电,最大电流能到多少?安卓手机能超过1.5A吗?苹果手机和iPAD能到2.4A吗?

2>基于上面的条件,此时USB2通路的D+/D-是悬空的,将这一路的TPS2549设置为(CTL1-3:001),此时能够进入DCP模式吗?如果可以的话,将R(ILIM_HI) 设置为 19.1 kΩ,这一路给支持快充的安卓手机,苹果手机,以及iPAD分别充电,最大电流能到多少?