This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2543 的应用问题

Other Parts Discussed in Thread: TPS2543

各位大虾,我在应用TPS2543 时遇到问题....能否给予解答...多谢

1.我在赛格电子市场上买回的TPS2543...原本设计是 CTL2,CTL3 ,ILIM_SEL 连接在一起,由一个I/O口控制(用A表示),CTL1 由另一个I/O口控制,(用B表示), EN 由另一个I/O口 控制( 用C表示),这样我想上电时,让A 为高,B为低,C 为高,进入DCP AUTO 模式,且有STATUS 状态检测负载的接入...当负载接入时,STATUS 为低,这样B输出高,

转为 CDP 模式,进行USB 通讯,但现在发现....无论B 是否为高或低..D+ 和D- 都是2.7 和2V ...不知为何?

 

2.另一个板上,是当B为高电平时,转为CDP模式,可以和USB 通讯,但是...此过程中,不管有无负载,STATUS 总为低电平,我上拉也为低电平,不知为何?