This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940的SYS_STAT[OVRD_ALERT]位一直无法写1清除

Other Parts Discussed in Thread: BQ76940

OVRD_ALERT (Bit 4): External pull-up on the ALERT pin indicator. Only active when ALERT pin is not already
being driven high by the AFE itself.
0 = No external override detected
1 = External override detected. Remains latched high until cleared by the host.
在ALERT引脚上下接470K欧电阻,并接470pF电容,接入MCU引脚配置为输入态,对BQ76940上电后读SYS_STAT状态值bit[4]一直为1,写入1亦无法消除,不知哪抽风了一直检测异常,望指导。