Hello Sir,
I have to use Bq28z610 IC and Soshine 1600mah and 3.6v. Design Capacity is12800mah(2s 8p) and 7.2v. Chemistry ID is 400
I completed two learning cycle process. The files are attached here(Learning cycle file and export gg file)
The full charge capacity value before the start of the first learning cycle process is 12601 mah (rest-exit-rest-charge-relaxation-discharge-rest). After completing the learning cycle, I checked the full charge capacity value. But this value was suddenly changed to 9173 mah. The full charge capacity value is 9173 mah before starting the second learning cycle process. But this time the same problem occurs and the value was suddenly changed to 9781 mah.
What is the reason for the sudden change in the value of the full charge capacity?
The same problem occurs and each time the value of Q MaxPassed Q and DOD0 pass Q is changed.
what is QMaxPassedQ and DOD0 Passed Q? Why was it changed every time?
Full charge capacity is not stable. every time the value(FCC) has changed. I need a standard full charge capacity value(12800 mah). Please help me