This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用UC2844和2843做的开关电源会有什么区别?

Other Parts Discussed in Thread: UC2844, UC2843

请问下,使用UC2844和2843做的开关电源会有什么区别?UC2844最大占空比50%,UC2843最大占空比100%,同一个反激式开关电源,输出路数电压电流一样,使用UC2844和UC2843最终结果会有哪些区别?

  • Hi
    在芯片datasheet第三页有一个对照表,从中你可以看到主要是供电,和占空比的差异。
    很明显,因为这些差异,很难同一个电路,2个芯片都可以用。你需要根据条件选择合适的芯片,例如假设最大duty只有不到50%,两个都可选,这个时候你还要确认供电是否满足。但是如果duty大于50%,就只能选择UC2843了。