This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2的外部TS1,2,3,4温度是怎么采样的?

Other Parts Discussed in Thread: BQ40Z50-R2

看BQ40Z50-R2的Datasheet 和Technical reference manual这两份文档里面都没有找到温度是怎么采的。

我的理解是这样,芯片内部用18KΩ电阻上拉到1.8V,外部加NTC分压,然后ADC会采这个电压值确定温度,那么采集到的电压值与NTC的阻值应该是有一个对应关系的,不同的NTC关系应该不一样。文档推荐用10KΩ@25℃的NTC,那么就应该内部有个标定,就是10K和18K分压时采到的电压值对应25℃,两份文档里面都没有提到怎么计算,只是说可以直接采集到温度值,这样的话我用不同的NTC在相同电阻下实际温度有可能是不一样的,那内部是怎么计算的呢?