我们使用TPS25200来作为USB的电源保护器件,在模拟USB过流保护的之后,拔出USB过流保护的故障源,FAULT引脚没有恢复为高电平,变成了持续的脉冲输出,需要重新断电重启才可恢复
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们使用TPS25200来作为USB的电源保护器件,在模拟USB过流保护的之后,拔出USB过流保护的故障源,FAULT引脚没有恢复为高电平,变成了持续的脉冲输出,需要重新断电重启才可恢复
Hi
The TPS25200 thermally protects itself by thermal cycling during an extended overcurrent condition. The device turns off when the junction temperature exceeds 135°C (typical) while in current limit. The device remains off until the junction temperature cools 20°C (typical) and then restarts. The TPS25200 cycles on/off until the overload is removed (see Figure 26 and Figure 29).
The FAULT signal is not deglitched when the MOSFET is disabled due to an overtemperature condition but is deglitched after the device has cooled and begins to turnon. This unidirectional deglitch prevents FAULT oscillation during an overtemperature event.