This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138PSFBEVM的PWR050A电路在Vin为405V时输出电压PIN6 Vinmonitor异常



您好。

我在测试UCD3138PSFBEVM开发板时,遇到一个异常现象。

手册中说Vin的过压保护点时410V,

当我测试vin为405V时,发现辅助电源板PWR050A的输出电压PIN3和PIN6等不稳定,出现振荡。

不知是什么原因?是PWR050A的R46电阻值偏小,高压空载时,反馈信号较弱易受干扰吗?

谢谢。