3.7V锂电池输入,如何获得12V,3A可调电流或者电压,采用Datasheet的典型电路,在没有负载情况下电压是正确值,如果有负载情况下,电压只有6V左右,先咨询下,按照datasheet的典型电路,如何求电流问题???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
3.7V锂电池输入,如何获得12V,3A可调电流或者电压,采用Datasheet的典型电路,在没有负载情况下电压是正确值,如果有负载情况下,电压只有6V左右,先咨询下,按照datasheet的典型电路,如何求电流问题???
您好
负载是4和个串联的3W的大功率LED管,现在目标是通过改变电压或者电流的方式,使其发光管能正常工作,正常工作状态下,电压典型值是2.2V~2.6V,单芯的电流是700mA,最大值是1A,现采用4个四芯灯珠串联,那边工作电压应该在8.8V~10.4V,最大可以达到11.2V将近12V,电路需要达到2.8A(典型值),故改变发光强度,那么电流范围应该在2A~4A可调,现拟采用3.7V锂电池供电,主要问题是如何改变反光管的亮度达到实验要求
谢谢