本人最近用TPS65131芯片做一个输入5V转±15V输出的电源电路,当输入为5V时实际输出为+4V和-1.25V,感觉芯片没有工作或输出电流不够导致输出电压被严重拉低。但是,根据TPS65131的数据手册其输出能力为15V/0.5A和-15V/0.3A),而我的负载为17片运放OPA2188和两片电压比较芯片LM393,无论如何TPS65131应该都可以满足要求。所以想请群里的大神帮忙分析一下是什么原因导致TPS65131工作不正常。电路图纸如下:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
回路,例如输入,电感,肖特基,输出,与GND 构成的回路。 输入,电感,MOS,GND又构成回路,这个回路路径上要求尽量小。