This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40170负载调整率异常

Other Parts Discussed in Thread: TPS40170

基于TPS40170设计的输入40-60V,输出5V@Max 12A 电源, 使用WEBENCH仿真过,并使用其参数设计的原理图(如下图)

实际测试时,发现两个问题:

1. 空载时芯片发热(热温枪测试,大约80°C),这个考虑在VIN的位置加1R的电阻,请问是否合适

2. 使用负载测试仪测试,当输出10A电流时,电压跌至4.3V,这个目前没有更好的解决办法,故请教下该如何调整最佳(环路稳定电路部分的参数调整过,但是依旧不行)