新型多串半桥谐振高效LED 驱动解决方案及其应用
下载观看:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大功率LED照明的新型双级多串LLC架构的优势可以总结为以下四点:第一,效率提升,这个新的拓扑架构实际总体效率可以达到92%。第二,成本很低,因为不需要每一串DC/DC的降压,TI用一串变压器可以驱动两串LED,两串变压器可以驱动四串LED,采用的变压器都是传统的变压器,成本远远低于用恒压的DC/DC对每一串进行驱动。
第三,它的元器件非常少,所以它的可靠性很好,把恒压和恒流整个集成在一个级上,而不是两个,使得可靠性得到提升。此外,传统驱动方案用的电容很多,因为每串DC/DC降压都需要电容,PFC也需要电容,LLC也需要电容。电容损坏也是影响LED路灯可靠性的一个重要因素。这个架构的电容数少,所以可靠性提升。
第四,EMI问题减小,设计更简单。电路没有多串的DC/DC,只需要一个谐振半桥实现驱动,这样可以非常容易地得到EMI设计。