This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3433怎么得到电流特性?



LM3433板子设计的是将LED灯直接插在板子上,哪怎么样能得到电流特性呢?直接检测LED电压特性是否就能反映出电流特性呢?我想串联一个分流器(50A,750mV),但是因为手册上说导线会有寄生电感,不敢上电,不知道这种方法行不行(电缆线,总长度大概是50cm,所要测试的是32KHz,30A电流),忘大神指点,小弟超级菜鸟,多谢。

  • Hi

      如果你是要测试LED的电流,可以用大功率的电流钩表。

     

  • LM3433是带高频调光的HBLED驱动器,为大功率LED提供了恒流照明.工作输入电压为-9V到-14V,输出电流大于6A,PWM频率大于30kHz,适用于共阳极LED,不需要输出电容,开关频率高达1MHz,静态电流典型值为1mA,具有软起动特性,可用于LCD背景光,投映系统,固态照明和汽车照明

  • LM3433是一款自适应恒定导通时间的DC/DC降压型输出恒流控制器,是针对高电流下驱动高亮度发光二极管(HBLED)而设计的产品。LM3433是一个真正的电流源,输出为恒定纹波的恒定电流,与LED正向压降的变化无关。

      以接地(GND)为参考,*估板可接受范围从-9V到-14V的输入电压。当输入为负电压时,为达到最大散热效率,输出配置允许多个LED的阳极并到一起,连到接参考地的机架上

  • 串一个电流表在回路中,然后监测输出电压,虽然会有些引线电感之类的,但影响非常小,基本可以忽略不计的

  • 按照评估板电路我做了一块板子 驱动电流为2A-6A的 但是NTMFS4841NH场效应管不能导通,GSD端的电压条件都符合导通要求。。。