This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq28z610如何限制最大容量Capacity



Design Capacity mAh是2000mAh, 做完循环学习和导出量产文件。由于每次充满电Full charger Capacity都会有差异, 设想的正常范围是1900mAh~2100mAh。新的电池,烧录了量产文件后,做反复充放电测试,有些时候出现这样的问题,循环充放电1~4次Full charger Capacity在正常范围内都能充到100%, 但第5次以后Full charger Capacity大于2200mAh,导致只能充到98%或者99%,  所以有没有办法限制Full charger Capacity的最大值, 限制在2100mAh以内?