BQ27542-G1的自学习 :
1. 电池放电直至空,静置5小时。
2. 向电量计发送IT ENABLE,VOK =1,UpdateStatus = 0x04
3. 将电池电充满,FC = 1,VOK =1 ,UpdateStatus = 0x04
4. 静置2小时 ,VOK = 0,UpdateStatus = 0x06,并且此时更新的Qmax和实际值相差太多,按照 《Reference manual》 P115
所述,UpdateStatus 应该为0x05,即Update Status:
Bit 0 (0x01) indicates that the fuel gauge learned an initial value for Qmax after the charging portion of
a learning cycle.
UpdateStatus 怎么会直接跳到0x06呢?