This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24707参考电路

Other Parts Discussed in Thread: BQ24707

BQ24707输入端的两个PMOS作用,我看到相关手册上说是防止适配器反接的,那为什么还要controled by host?是还有其他作用吗?我这里实际测试的结果是只要插上适配器,然后通过I2C写入寄存器后充电就开始了,不论这两个PMOS管的G极是什么状态。所以他们的作用到底是什么?

  • Q1是输入保护MOSFET
    Q2是防倒灌保护MOSFET,若没有这个MOSFET,电流能通过Q1的体二极管倒灌到输入源。从电路图可以看到,Q1和Q2之后就是系统输出端(系统负载),如果没有Q1,开机时,系统输出端的电容会使得输入源承受很大的电流应力,因为这些容性负载而出现一个很大的涌浪电流,甚至使得输入源被瞬间拉低,而芯片的UVLO恰好是要检测输入源直接输入端AVCC,所以甚至会造成启动时出现错误的欠压保护,加入Q1以后,因为MSOFET 的开启特性,所以在其g-s电压逐渐向开启电压转变至过驱动的过程中, 输入电流是缓慢的增加的, 就不会在瞬间拉低输入源。同时也可以通过额外的g-s g-d来进一步的使得启动过程更加平滑。
  • 非常感谢!Q1我已经明白了,可是Q2防倒灌还是不太清楚,电流是怎样倒灌进输入源的?还有Q2为什么要host来控制?
  • 非常感谢!Q1我已经明白了,可是Q2防倒灌还是不太清楚,电流是怎样倒灌进输入源的?还有Q2为什么要host来控制?
  • 您好,Q2用作反向阻断FET,可在没有适配器的情况下防止任何电流流回输入端。