This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176调试低电压输入带不起负载

Other Parts Discussed in Thread: LM5176

我们现在使用LM5176出现以下问题,请帮忙处理:输出电压12V

在13Vdc输入电压时,只能带6.5A电流。在24Vdc输入电压时,可以带25A电流,但是老化5分钟后,输出电压会跌下来去到8V左右;如果遇到这种情况,能从哪个地方入手调好?

  • Hi
    首先要确认功率电感饱和电流足够,24V能在降压下带25A, 但是如果是在升压下呢? 如果仍要25A, 电感饱和电流需要更大。在老化时,还需要确认到板子上的13V电压,不会瞬态拉低,这样会造成电感上的电流更大,更易饱和。
    同时也要注意功率电感是否受老化房高温影响比较到(本身大电流会造成电感一定程度的发烫,叠加老化房高温是否有问题)