我们使用TPS65910AA1给AM3359供电,实测发现提供给MPU的电压为1.1V(理论上应该是1.26V),因为我们是在电子市场买的散货,不知道是不是买错型号了,有没有哪颗料的VCC1是默认1.1V输出的,或者有没有什么方法可以确认一下这种问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们使用TPS65910AA1给AM3359供电,实测发现提供给MPU的电压为1.1V(理论上应该是1.26V),因为我们是在电子市场买的散货,不知道是不是买错型号了,有没有哪颗料的VCC1是默认1.1V输出的,或者有没有什么方法可以确认一下这种问题。
Hi
见AM335x 的使用指导: http://www.ti.com.cn/general/cn/docs/lit/getliterature.tsp?literatureNumber=swcu093b&fileType=pdf
TPS65910A/TPS65910A3/TPS65910A31A1 的VDD1 默认输出都是1.1V.
如果是买错了,还有的救吗?
显示有IIC总线可以改,是实时生效的么?
我设置的boot[1:0]=10(官方推荐的连法),使用EEPROM的参数,我自己可以改吗?
boot[1:0]=00和boot[1:0]=01都不适合AM335X的。
看了一下芯片的丝印,第一行是“T65910A”,第二行是“A1”,对比了一下datasheet,应该没买错型号,会跟主芯片相关吗?丝印是“AM3359ZCZD72”
问题已解决,原来TPS65910AA1默认就是1.1V的输出,uboot加载成功后才会变到1.26V。