Other Parts Discussed in Thread: BQ24103, BQ24103A, BQ24170
求推荐几款两串的7.4V聚合物锂电池充电芯片!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
充电指示对于每一个集成的充电器芯片而言是都有的。线性充电器的优点在于电路结构简单,外部器件少,占PCB的面积也很少,成本相对比较小。开关模式充电器与线性充电器相比最大的优点在于当输入电压和输出电压相差比较大时效率能比线性充电器提高很多。对于线性充电器,忽略偏置电流等的影响,其效率可以用vout/vin来评估,其内部调整管消耗的功率可以用Iout*(Vin-Vout)来评估,所以我们可以看到当输入电压与输出电压比较大时,线性充电器效率非常低,且当充电电流比较大时,调整管消耗的功率非常大,这意味着芯片的温度也会非常高。
关于您的这个项目,BQ2057T能满足你的需求,但效率粗略评估只有不到70%;如果贵司的项目希望有更高的效率,则使用BQ24103A 。
这两款芯片比较起来,最大的区别有以下两点
1:BQ24170具有power path,这说明它支持充电器插入时一边给电池充电,一边给系统负载供电;而BQ24103A只是单纯的给电池充电,不具备功率路径的管理,所以如果你的项目要求充电器插入时,由充电器给负载供电,充电器未插入时自动切换到电池给负载供电,则选择BQ24170,如果你只是单纯的做一个充电器BQ24103A也是比较不错的选择。
2:关于CC模式下的充电电流,BQ24170最大支持4A,而BQ24103A只有2A,从你提供的适配器最大2A的输出电流来看,你的CC电流应该会保留一定的俗量,所以这两个器件对于充电电流的限制上都是满足你需求的。