Other Parts Discussed in Thread: LM73605, LM76005
你好,
我在最近的应用中需要将15V~36V的输入降压到13V,电流在4A以下,我想要对比LM73605和LM76005的方案,请问这两个芯片各自的优劣在哪?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
优劣不好说,建议说合适和更合适,对于实现同样功能转换的电源芯片,各有优劣,最重要的是选择最适合你需求的。
相比较而言LM73605只是36Vmax输入的芯片,如果你的应用中输入可能到36V,建议你选择LM76005, 或者至少比36V略高输入的芯片。这个芯片优势在于频率范围大,可以设计极高的频率,使得电感感量相对较小,减小体积。