This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq40z50 learning cycle 中电压电流选择问题

Other Parts Discussed in Thread: BQ40Z50-R2

Hi Team,

       bq40Z50-R2 , 3S1P电池,电池放到9V时,能放出6000mAh,terminate voltage为10.8V ,满充放电到10.8V能放出4600mAh ,在做learning cycle 时有些疑问

      1.开始充电电压是9V-9.9V之间还是10.8V左右?

      2.充电电流0.5C ,放电电流0.2C是按照6000mAh计算还是按照4600mAh计算?

      3.放电周期的放电截止电压是到terminate voltage 10.8V 还是放到9V左右?

  • 您好,
    1, 建议您将电池放空以后充一会儿手动量一下。因为电压在CC模式是虚高的,将电源断开电池电压就会降下来。
    2,3,建议您参考电芯的规格书

  • 2,3两点讲的都是学习的时候,SLUA597中讲到要充满搁置2小时放空搁置5个小时,放空的时候提到了the battery relaxes to a low (~3.0–3.3V) voltage 和: Make sure that when terminate voltage is reached, the load is removed .Let the cell relax 两个说法 不知道以哪个为准,终端电压3.6(单节)这时候大概还有1400mah ,relax 5 个小时电压不会到达3.0—3.3之间
  • 您好,没有 找到SLUA597这个 文档。充满搁置2小时放空搁置5个小时前提是要确保电池有效的 满充和放空。
    电池放空以后将load移除,会发现电压有回升现象,所以才有上面两点,建议同时满足两个条件。