This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有关LM3424芯片引脚CSH电压



CSH引脚电压看说明是最高1.26V,正常计算取值为1.24V,我实现做出来的板子,测试CSH引脚电压是1.29V

这个1.29V是不是不正常,会是什么引起的电压比正常值要大?

  • Hi
    1.29V是偏高的,如果万用表测量,你可以用示波器测试看一下。
    有可能是你选择GND的问题,这里建议选择模拟GND,不要选择电流较大的功率GND. (可以看一下datasheet第62页,是有将功率GND单独出来,其余的就是模拟GND了。注意注意功率回路)