This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76005的efficiency疑惑

Other Parts Discussed in Thread: LM76005

Hi Ti,

   我期望用LM76005输入一个48V电压,然后输出40V 4A的电源。用WEBENCH® Designer设计图形如下:

看了一眼别的设计还好,但是efficiency到了98%。看了看手册明确写了95% efficiency at 400 kHz (12VIN, 5VOUT, 2A)。我想问问,这个工具设计的可行性有多少?按照工具的设计真能让LM76005的efficiency达到98%吗?

谢谢!

  • Hi
    应该是可以接近的。不同条件效率略有差异,效率做到98%是可能的(不过这个一般是峰值效率),但是要注意要尽量按照webench里的器件选型或者选择更低功耗的。
  • Hi
    应该是可以接近的。不同条件效率略有差异,效率做到98%是可能的(不过这个一般是峰值效率),但是要注意要尽量按照webench里的器件选型或者选择更低功耗的。
x 出现错误。请重试或与管理员联系。