Other Parts Discussed in Thread: BQ25895
请问我在使用BQ25895充电芯片时,即使将寄存器中的ICHG设置为5A,IINLIM设置为3.25A,在使用直流电源供电的情况下充电电流最大只能到约2.2A。在使用支持快充的充电器时,检查寄存器识别充电器类型为Adjustable High Voltage DCP (MaxCharge) (1.5A),但是充电电流仍然仅为约2A。
请问:
1、是否可以通过寄存器设置强制使充电电流到5A,如何设置。
2、如果必须通过充电器的握手才能到5A充电,请问什么规格或协议的充电器才能达到5A充电。
下图是测试平台的照片,请参考:
谢谢!