这里需要使用 3.7V 升压至 36V 进行mA级别的电流输出,由于没找到合适的DCDC芯片,所以采用两路DCDC进行级联。3.7V升压到12V,再用12V升压到36V。用的也都是TI的片子。在使用时发现单独测试DCDC模块都能正常工作,但是一旦级联以后,即使36V端需要输出的电流值为1~2mA,在3.7V也会出现比较严重的电压拉低情况,并且其频率和12V升压到36V芯片的开关频率非常接近。怎么消除这个启动时的输入源电压拉低现象呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这里需要使用 3.7V 升压至 36V 进行mA级别的电流输出,由于没找到合适的DCDC芯片,所以采用两路DCDC进行级联。3.7V升压到12V,再用12V升压到36V。用的也都是TI的片子。在使用时发现单独测试DCDC模块都能正常工作,但是一旦级联以后,即使36V端需要输出的电流值为1~2mA,在3.7V也会出现比较严重的电压拉低情况,并且其频率和12V升压到36V芯片的开关频率非常接近。怎么消除这个启动时的输入源电压拉低现象呢?