This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6735的5V转-5V的最大输出电流不够

Other Parts Discussed in Thread: TPS6735

您好!

在运用TPS6735的5V转-5V的方案时,实际测量最大输出电流为0.095mA,与技术手册中的200mA相差有一些远,满载工作时芯片温度为34.4℃,不清楚什么原因达不到数据手册的最大输出电流。